Keysight 89600 VSA .NET API
PropertyNames Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > ProcessingExtension Class : PropertyNames Method


Glossary Item Box

Gets an array of the valid property names.

Syntax

Visual Basic (Declaration) 
Public Overridable Function PropertyNames() As String()
C# 
public virtual string[] PropertyNames()
C++/CLI 
public:
virtual array<String^>^ PropertyNames(); 

Return Value

The array of names.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 20.00

See Also