| Visual Basic (Declaration) | |
|---|---|
Public MustOverride ReadOnly Property PlayDelaySec As Double | |
| C# | |
|---|---|
public abstract double PlayDelaySec {get;} | |
The trigger delay of the recording is the same as the trigger delay of the inputs when the data was recorded. The delay is zero if the trigger was free run.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)