| | Name | Description | Minimum SW Version |
 | CurrentFileName | Gets the current recording file name. | — |
 | IsDisposed | Gets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
 | IsMultifileRecording | Gets a value indicating whether the source for the current recording in VSA is from multiple recording files. | 28.00 |
 | IsPlayLoop | Gets or sets a value indicating whether playback of the recording will loop to the starting point when it reaches the stopping point. | — |
 | IsPlaySegmentedCapture | Gets a value indicating whether the current recording is a segmented capture. | 19.00 |
 | IsPlayZoom | Gets a value indicating whether the current recording is zoomed. | — |
 | IsRecordLengthExtra | Gets or sets a value indicating whether extra data will be acquired to be able to settle the measurement filters during playback. | — |
 | IsRecordLengthMaximum | Gets or sets a value indicating whether the recording length will be the maximum supported by the input channels. | — |
 | PlayCenter | Gets the current recording center frequency. | — |
 | PlayChannels | Gets a handle to a collection of PlayChannel objects | — |
 | PlayDelaySec | Gets the trigger delay (in Sec) of the current recording. | — |
 | PlayDeltaSec | Gets the delta time (in Sec) between sample points in the current recording. | — |
 | PlayMaxSpan | Gets the cardinal frequency span of the current recording. | — |
 | PlayPoints | Gets the number of points in the current recording. | — |
 | PlayPointsHuge | Gets the number of points in the current recording. | 23.00 |
 | PlayPosition | Gets or sets the current point of the recording playback. | — |
 | PlayPositionHuge | Gets or sets the current point of the recording playback. | 23.00 |
 | PlaySampleRate | Gets the sample rate (in Samples/Sec) of the current recording. | — |
 | PlaySegmentCount | Gets the number of segments in the current recording. | 19.00 |
 | PlaySegmentType | Gets the current recording segment type in the current file being used for playback. The value returned is only valid if it is a segmented capture recording file. | 25.40 |
 | PlaySpan | Gets the frequency span, in Hertz, of the current recording. | — |
 | PlayStart | Gets or sets the starting point of the recording playback. | — |
 | PlayStartHuge | Gets or sets the starting point of the recording playback. | 23.00 |
 | PlayStartSec | Gets or sets the starting time of the recording playback. | — |
 | PlayStop | Gets or sets the stopping point of the recording playback. | — |
 | PlayStopHuge | Gets or sets the stopping point of the recording playback. | 23.00 |
 | PlayStopSec | Gets or sets the stopping time of the recording playback. | — |
 | RecordLength | Gets or sets the length of the next recording. | — |
 | RecordLengthMaximumTime | Gets the maximum recording time supported by the current measurement's input channels. | — |
 | RecordLengthTime | Gets the time length of the next recording. | — |
 | RecordLengthUnit | Gets or sets the units of the length of the next recording. | — |
 | SavedFileName | Gets the file name that the current recording was last saved to (or recalled from). When recalling multiple files SavedFileName has a semicolon separated list of the recalled files. | — |
 | SegmentedCaptureDuration | Gets or sets the recording-specific segmented-capture duration (or timeout), in seconds. | 31.00 |
 | SegmentedCaptureDurationAuto | Gets or sets a value indicating whether SegmentedCaptureDuration is computed automatically. | 31.00 |
 | Trigger | Gets a handle to the ITrigger object for playback. | — |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. |