| Visual Basic (Declaration) | |
|---|---|
Public Overridable Sub RecallMultifile( _ ByVal fileNames() As String, _ ByVal format As String, _ ByVal paddingType As RecordPaddingType, _ ByVal padding As Single _ ) | |
| C# | |
|---|---|
public virtual void RecallMultifile( string[] fileNames, string format, RecordPaddingType paddingType, float padding ) | |
| C++/CLI | |
|---|---|
public: virtual void RecallMultifile( array<String^>^ fileNames, String^ format, RecordPaddingType paddingType, float padding ) | |
Parameters
- fileNames
- Specifies the files to recall.
- format
- Specifies the file format.
- paddingType
- Specifies the type of padding to perform.
- padding
- Specifies the amount of padding (interpretation of this parameter depends on the paddingType).
The current recording, in SDF format, is overwritten. SetCenterSpan is called as part of this method.
Supported File Formats:
| format | Description |
|---|---|
| "CSV" | CSV (Comma delimited) [*.csv] |
| "MAT" | MAT-File [*.mat] |
| "MAT7" | MAT-File (HDF5) [*.mat, *.hdf, *.h5] |
| "TEXT" | Text (Tab delimited) [*.txt] |
| "VITA49" | VITA 49 [*.vita49] |
Note:
MAT may be used instead of MAT7 for recall trace/recording (the matlab file format is auto detected for recall).
For more information about file types, see the "Supported File Formats" topic in the application help.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.00