Keysight 89600 VSA .NET API
SetRecordLength Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Recording Class : SetRecordLength Method


length
Specifies the length of the recording.
unit
Specifies the unit as either, second, record, point, or segment.

Glossary Item Box

Set the length (with its unit) of the next recording.

Syntax

Visual Basic (Declaration) 
Public MustOverride Sub SetRecordLength( _
   ByVal length As Double, _
   ByVal unit As RecordLengthUnit _
) 
C# 
public abstract void SetRecordLength( 
   double length,
   RecordLengthUnit unit
)
C++/CLI 
public:
abstract void SetRecordLength( 
   double length,
   RecordLengthUnit unit
) 

Parameters

length
Specifies the length of the recording.
unit
Specifies the unit as either, second, record, point, or segment.

Remarks

If the IsRecordLengthMaximum is set to True, then the recording length is set to the largest size that the inputs will support. This is limited by capabilities of the input channel hardware, including how much memory is installed in the hardware.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also