Keysight 89600 VSA .NET API
RemotableObject Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : RemotableObject Class

Glossary Item Box

The following tables list the members exposed by RemotableObject.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public Methodstatic (Shared in Visual Basic)BuildExceptionMessageBuild an error message string from the supplied System.Exception object, including information from inner exception(s) and System.TypeLoadExceptions.  —
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection.  —
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceOverridden. Obtains a lifetime service object to control the lifetime policy for this instance.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes.  —
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes.  —
Public EventRemotePropertyChangedOccurs when a property value changes.  —
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes.  14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also