Keysight 89600 VSA .NET API
RemoteCollectionChangedEventArgs Class Members
See Also  Properties 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : RemoteCollectionChangedEventArgs Class

Glossary Item Box

The following tables list the members exposed by RemoteCollectionChangedEventArgs.

Public Constructors

 NameDescriptionMinimum SW Version
Public ConstructorRemoteCollectionChangedEventArgs ConstructorInitializes a new instance of the RemoteCollectionChangedEventArgs class.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyActionGets the action that caused the event.  —
Public PropertyNewItemsGets the list of new items involved in the change.  —
Public PropertyNewStartingIndexGets the index at which the change occurred.  —
Public PropertyOldItemsGets the list of items affected by a Replace, Remove, or Move action.  —
Public PropertyOldStartingIndexGets the index at which a Move, Remove, or Replace action occurred.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also