Keysight 89600 VSA .NET API
OldStartingIndex Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > RemoteCollectionChangedEventArgs Class : OldStartingIndex Property


Glossary Item Box

Gets the index at which a Move, Remove, or Replace action occurred.

Syntax

Visual Basic (Declaration) 
Public ReadOnly Property OldStartingIndex As Integer
C# 
public int OldStartingIndex {get;}
C++/CLI 
public:
property int OldStartingIndex {
   int get();
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also