| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property CarrierPhaseOffset As Double | |
| C# | |
|---|---|
public virtual double CarrierPhaseOffset {get; set;} | |
This property is used to adjust the phase difference between carrier frequencies of downloaded waveforms on a source with multiple channels. Sources that support digital up conversion use Frequency to set the carrier frequency.
The IsSupported("CarrierPhaseOffset") method can be used to determine whether this property is supported or not with the current Source.SelectedHardware.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.40