| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property Frequency As Double | |
| C# | |
|---|---|
public abstract double Frequency {get; set;} | |
When the source is an arbitrary waveform generator (AWG), this property is read-only. Its value is set during download to the WaveformCenterFrequency value applied to the downloaded waveform, which may be rounded to maintain phase continuity.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)