| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property WaveformCenterFrequency As Double | |
| C# | |
|---|---|
public virtual double WaveformCenterFrequency {get; set;} | |
The value of this property is applied when a waveform is downloaded to an AWG./>
Phase continuity of a waveform being played by an AWG depends on the relationship between the duration in time of the waveform being downloaded and the waveform center frequency. To maintain phase continuity while playing the waveform, the waveform center frequency in Hertz must be an integer multiple of the reciprocal of the waveform duration in seconds. The value of this property is rounded to the nearest frequency that maintains phase continuity when a waveform is downloaded. Frequency is set to the rounded waveform center frequency applied to the downloaded waveform.
The IsSupported("WaveformCenterFrequency") method can be used to determine whether this property is supported or not with the current Source.SelectedHardware.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.00