Keysight 89600 VSA .NET API
IQOutput Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > SourceChannel Class : IQOutput Property


Glossary Item Box

Gets the I/Q output of this source channel, or null if I/Q output is not supported.

Syntax

Visual Basic (Declaration) 
Public Overridable ReadOnly Property IQOutput As IQOutput
C# 
public virtual IQOutput IQOutput {get;}
C++/CLI 
public:
virtual property IQOutput^ IQOutput {
   IQOutput^ get();
}

Remarks

A non-null return value indicates the source channel is capable of driving I and Q baseband output connectors directly. Most source instruments return null.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 31.00

See Also