| Visual Basic (Declaration) | |
|---|---|
Public Overridable ReadOnly Property VirtualSignals As VirtualSignalCollection | |
| C# | |
|---|---|
public virtual VirtualSignalCollection VirtualSignals {get;} | |
| C++/CLI | |
|---|---|
public: virtual property VirtualSignalCollection^ VirtualSignals { VirtualSignalCollection^ get(); } | |
The size of the collection depends on the number of virtual signals that the source supports for each of its channels. Virtual signals may be a licensed feature of a source. For example, M9484C supports virtual signals with Option 8SG. The collection is empty if the source does not support virtual signals.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00