Keysight 89600 VSA .NET API
Operation Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > SourceLogicalChannel Class : Operation Property


Glossary Item Box

Gets the operation that is done when combining the inputs within this logical channel.

Syntax

Visual Basic (Declaration) 
Public MustOverride ReadOnly Property Operation As LogicalChannelOperation
C# 
public abstract LogicalChannelOperation Operation {get;}
C++/CLI 
public:
abstract property LogicalChannelOperation Operation {
   LogicalChannelOperation get();
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also