Keysight 89600 VSA .NET API
SourceLogicalChannel Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : SourceLogicalChannel Class

Glossary Item Box

The following tables list the members exposed by SourceLogicalChannel.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAmplitudeGets or sets the source output power (dBm) for this channel.  —
Public PropertyChannelTypeGets the type of logical channel.  —
Public PropertyDisplayNameGets the display name for this logical channel.  —
Public PropertyFrequencyGets or sets the source RF frequency (Hertz) of this channel.  —
Public PropertyIdGets a unique identifier for this logical channel (within the context of the current hardware).  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsModulationOnGets or sets a value indicating whether to turn on I/Q modulation for this channel.  —
Public PropertyIsRFOnGets or sets a value indicating whether to true on RF output for this channel.  —
Public PropertyOperationGets the operation that is done when combining the inputs within this logical channel.  —
Public PropertyPhysicalChannelsGets a collection of the physical source channels that form this logical channel.  —
Public PropertyWaveformCenterFrequencyGets or sets the waveform center frequency (Hertz) set on this channel during download to an arbitrary waveform generator (AWG)  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also