Keysight 89600 VSA .NET API
FloatDataAtScan Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Spectrogram Class : FloatDataAtScan Method


scan
Specifies the spectrogram scan.

Glossary Item Box

Gets the raw data as a float array at the specified scan index.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function FloatDataAtScan( _
   ByVal scan As Integer _
) As Single()
C# 
public abstract float[] FloatDataAtScan( 
   int scan
)
C++/CLI 
public:
abstract array<float>^ FloatDataAtScan( 
   int scan
) 

Parameters

scan
Specifies the spectrogram scan.

Return Value

A float array

Remarks

All scans have the same format as the Trace's FloatData, which contains the data for the current scan.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also