Keysight 89600 VSA .NET API
Spectrum Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : Spectrum Class


Glossary Item Box

The Spectrum object contains members for controlling the power spectrum measurement features.

Object Model

Spectrum ClassSpectrumFrequency ClassSpectrumFrequencyChannelCollection ClassSpectrumFrequencyChannel ClassInputGate ClassInputGateChannelCollection ClassInputGateChannel ClassSpectrumTrigger Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class Spectrum 
   Inherits RemotableObject
   Implements IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged 

Remarks

The Spectrum object represents settings specific to power spectrum measurements, including center frequency, span, RBW, VBW and their related settings and detectors. Some of these settings are found in the Frequency sub-object.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also