Keysight 89600 VSA .NET API
SpectrumFrequency Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : SpectrumFrequency Class


Glossary Item Box

The Frequency object contains members for controlling the power spectrum measurement frequency features.

Object Model

SpectrumFrequency ClassSpectrumFrequencyChannelCollection ClassSpectrumFrequencyChannel Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class SpectrumFrequency 
   Inherits RemotableObject
   Implements IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged 
C++/CLI 
public ref class SpectrumFrequency abstract : public RemotableObject, IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged  

Remarks

The Spectrum object represents settings specific to power spectrum measurements, including center frequency, span, RBW, VBW and their related settings.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.50

See Also