Keysight 89600 VSA .NET API
IsSpanToResolutionBandwidthRatioAuto Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > SpectrumFrequencyChannel Class : IsSpanToResolutionBandwidthRatioAuto Property


Glossary Item Box

Gets or sets a value indicating whether the SpanToResolutionBandwidthRatio is automatically set.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsSpanToResolutionBandwidthRatioAuto As Boolean
C# 
public abstract bool IsSpanToResolutionBandwidthRatioAuto {get; set;}
C++/CLI 
public:
abstract property bool IsSpanToResolutionBandwidthRatioAuto {
   bool get();
   void set (    bool value);
}

Remarks

When true, the SpanToResolutionBandwidthRatio property will be set to a value of 106. This property defaults to true.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also