Keysight 89600 VSA .NET API
SpanToResolutionBandwidthRatio Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > SpectrumFrequencyChannel Class : SpanToResolutionBandwidthRatio Property


Glossary Item Box

Gets or sets the ratio of span to resolution bandwidth.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property SpanToResolutionBandwidthRatio As Double
C# 
public abstract double SpanToResolutionBandwidthRatio {get; set;}
C++/CLI 
public:
abstract property double SpanToResolutionBandwidthRatio {
   double get();
   void set (    double value);
}

Remarks

This property will be coerced to a value of 106 when the IsSpanToResolutionBandwidthRatioAuto property is set to true.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also