| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property Span As Double | |
| C# | |
|---|---|
public abstract double Span {get; set;} | |
The SetCenterSpan method can be used to specify center and span all at the same time.
With version 19.00 or greater if this property is set to zero then the measurement operates in time-domain (zero span) mode and trace results for it are versus time instead of frequency. This is only supported though if the hardware supports it.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)