Keysight 89600 VSA .NET API
IsEquivalentSweepTimeAuto Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > SpectrumFrequency Class : IsEquivalentSweepTimeAuto Property


Glossary Item Box

Gets or sets a value indicating whether the equivalent sweep time is automatically chosen.

Syntax

Visual Basic (Declaration) 
Public Overridable Property IsEquivalentSweepTimeAuto As Boolean
C# 
public virtual bool IsEquivalentSweepTimeAuto {get; set;}
C++/CLI 
public:
virtual property bool IsEquivalentSweepTimeAuto {
   bool get();
   void set (    bool value);
}

Remarks

This property is ignored when in zero span mode.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also