Keysight 89600 VSA .NET API
VideoBandwidth Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > SpectrumFrequency Class : VideoBandwidth Property


Glossary Item Box

Gets or sets the video bandwidth in Hz. This is the -3 dB bandwidth.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property VideoBandwidth As Double
C# 
public abstract double VideoBandwidth {get; set;}
C++/CLI 
public:
abstract property double VideoBandwidth {
   double get();
   void set (    double value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.50

See Also