Keysight 89600 VSA .NET API
Holdoff Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > SpectrumTrigger Class : Holdoff Property


Glossary Item Box

Gets or sets the gate trigger holdoff in seconds.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property Holdoff As Double
C# 
public abstract double Holdoff {get; set;}
C++/CLI 
public:
abstract property double Holdoff {
   double get();
   void set (    double value);
}

Remarks

Determine the length of the trigger holdoff, in seconds. The holdoff is the length of time that the trigger condition must not be satisfied before accepting a trigger. For a positive trigger slope, it is the length of time that the input signal amplitude must be less than the trigger level before a valid trigger can occur. A larger trigger holdoff makes the trigger less susceptible to a momentary signal glitch.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also