Keysight 89600 VSA .NET API
SpectrumTrigger Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : SpectrumTrigger Class

Glossary Item Box

The following tables list the members exposed by SpectrumTrigger.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyDelayGets or sets the gate trigger delay in seconds.  19.00
Public PropertyExternalLevelGets or sets the external trigger level in volts.  19.00
Public PropertyHoldoffGets or sets the gate trigger holdoff in seconds.  19.00
Public PropertyHoldoffStyleGets or sets the gate trigger holdoff style.  19.00
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyMagnitudePowerLevelGets or sets the magnitude trigger level in dBm for the specified input channel.  19.00
Public PropertyPxiSourceGets or sets which PXI backplane trigger to use when the Source property is set to Pxi.  19.00
Public PropertyRFBurstLevelGets or sets the trigger level in dBm for the RF Burst trigger  19.00
Public PropertySlopeGets or sets the trigger slope.  19.00
Public PropertyStyleGets or sets the trigger style.  19.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also