| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property MagnitudePowerLevel As Double | |
| C# | |
|---|---|
public abstract double MagnitudePowerLevel {get; set;} | |
This is normally an in-channel trigger that is after resampling/decimation of data.
This property is only used if the trigger source is set to MagnitudeLevel.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00