Keysight 89600 VSA .NET API
TimeVersusTimeChannel Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : TimeVersusTimeChannel Class


Glossary Item Box

This class is for channelized TimeVersusTime parameters.

Syntax

Visual Basic (Declaration) 
Public MustInherit Class TimeVersusTimeChannel 
   Inherits RemotableObject
   Implements IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged 
C++/CLI 
public ref class TimeVersusTimeChannel abstract : public RemotableObject, IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged  

Remarks

The channels represented by this class are logical channels, which may be combinations of multiple physical hardware channels.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.40

See Also