| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property FastTimeLength As Double | |
| C# | |
|---|---|
public abstract double FastTimeLength {get; set;} | |
This value is used for fast-time slow-time measurements, where the fast-time refers to the number of range bins for a given slow time sample. The fast-time dimension has a higher sampling rate than the slow-time dimension. The slow-time length is determined by the capture length. and for how the capture length is determined. The default value is 10us.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.40