Keysight 89600 VSA .NET API
MaxAnalysisPointsAuto Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > TimeVersusTimeChannel Class : MaxAnalysisPointsAuto Property


Glossary Item Box

Gets or sets a value indicating whether the maximum number of analysis points should be automatically determined.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property MaxAnalysisPointsAuto As Boolean
C# 
public abstract bool MaxAnalysisPointsAuto {get; set;}
C++/CLI 
public:
abstract property bool MaxAnalysisPointsAuto {
   bool get();
   void set (    bool value);
}

Remarks

This setting is a boolean used to determine if the MaxAnalysisPoints is automatically configured. The default value is true.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also