| Overload | Description |
|---|---|
| ArrangeWindows(ArrangeWindowHints) | Arranges the trace windows on the display. |
| ArrangeWindows(ArrangeWindowHints,Int32,Int32) | Arranges the trace windows on the display. |
| ArrangeWindows(ArrangeWindowHints,IEnumerable<Measurement>) | Arranges the trace windows on the display. |
| ArrangeWindows(ArrangeWindowHints,Int32,Int32,IEnumerable<Measurement>) | Arranges the trace windows on the display. |
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)