Keysight 89600 VSA .NET API
IsGrid Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > TraceCollection Class : IsGrid Property


Glossary Item Box

Gets or sets a value indicating whether the grid (graticule) of the traces are visible.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsGrid As Boolean
C# 
public abstract bool IsGrid {get; set;}
C++/CLI 
public:
abstract property bool IsGrid {
   bool get();
   void set (    bool value);
}

Remarks

Determine whether the grid lines on all traces are Visible.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also