| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property IsXCenterSpanPowerSpectrum As Boolean | |
| C# | |
|---|---|
public virtual bool IsXCenterSpanPowerSpectrum {get; set;} | |
Returns whether all the PowerSpectrum traces have an X axis that displays the center and span frequencies, or the start and stop frequencies. This setting has no effect on a trace if it does not contain PowerSpectrum frequency domain data, is shown in I-Q or constellation format, or the X axis is scaled (IsXScaleAuto is set to False).
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.50