Keysight 89600 VSA .NET API
SelectedItem Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > TraceCollection Class : SelectedItem Property


Glossary Item Box

Gets or sets the selected Trace.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property SelectedItem As Trace
C# 
public abstract Trace SelectedItem {get; set;}
C++/CLI 
public:
abstract property Trace^ SelectedItem {
   Trace^ get();
   void set (    Trace^ value);
}

Remarks

The selected trace has the keyboard focus. Returns null if no trace is selected.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also