| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property Coupling As TraceCoupling | |
| C# | |
|---|---|
public virtual TraceCoupling Coupling {get; set;} | |
| C++/CLI | |
|---|---|
public: virtual property TraceCoupling Coupling { TraceCoupling get(); void set ( TraceCoupling value); } | |
Trace coupling determines whether this trace tracks changes in other traces' parameters (such as y-axis limits). Coupling is performed for traces that are placed into the same tab group and overlaid.
The following parameters can be coupled:
When Coupling = Automatic and a trace is placed into an overlay group, the VSA will attempt to set the coupling parameters automatically.
Auto coupling will be performed in these circumstances:
- Trace Overlay setting is enabled
- A trace is added to a tab group (drag and drop)
- A different trace data is selected for a trace
- Display layout is changed
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 20.0