| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property DataName As String | |
| C# | |
|---|---|
public abstract string DataName {get; set;} | |
The DataName property sets or returns the string that identifies a data source for this trace. The DataName is spelled differently than the trace data title (DataTitle property) that shows in the window title of the trace window. The trace data label name is modified for clarity, this may include additional spaces, demod type information, etc.
You can use the output window to find out what the active trace data name is; Open the output window (Click Window > Output), select the "Show Code" check box in the Output window, and then do the steps to specify a trace data. The output window shows the code to set the trace data name. You can also use the TraceCollection.DataNames property to return an array containing all the current possible data sources. If you are only interested in a subset of the available sources, use DataNamesMeasurements, TraceCollection.DataNamesMath, TraceCollection.DataNamesGraph, TraceCollection.DataNamesDataRegister, or TraceCollection.DataNameNoData to return only the Measurement, Math Functions, Graphs, or Registers sources, or the name No Data, respectively.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)