| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property Level As Double | |
| C# | |
|---|---|
public abstract double Level {get; set;} | |
The maximum input trigger level is dependent upon hardware and range and may be changed when the input range changes.
This property is only used if the trigger style is set to Level.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)