Keysight 89600 VSA .NET API
UserCorrection Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : UserCorrection Class


Glossary Item Box

The UserCorrection class has properties that allow user defined corrections to be applied to the data.

Object Model

UserCorrection ClassPlaybackUserCorrection ClassPlaybackUserCorrectionChannelCollection ClassPlaybackUserCorrectionChannel ClassPlaybackUserCorrectionLogicalChannelCollection ClassPlaybackUserCorrectionLogicalChannel Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class UserCorrection 
   Inherits RemotableObject
   Implements IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged 
C++/CLI 
public ref class UserCorrection abstract : public RemotableObject, IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.00

See Also