Keysight 89600 VSA .NET API
UserInputAcquisitionStatus Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : UserInputAcquisitionStatus Enumeration


Glossary Item Box

Acquisition status flags to support UserInputData.AcquisitionStatus.

Syntax

Visual Basic (Declaration) 
Public Enum UserInputAcquisitionStatus 
   Inherits System.Enum
C# 
public enum UserInputAcquisitionStatus : System.Enum 
C++/CLI 
public enum class UserInputAcquisitionStatus : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AcquiringDataAcquisition data source is acquiring data.—
IdleAcquisition data source is idle.—
NoneNo acquisition data source status information.—
TransferringDataAcquisition data source is transferring data to UserInputData.—
WaitingForTriggerAcquisition data source is waiting for a trigger event to occur.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Remarks

Acquisition status flags indicate the status of sending data into UserInputData.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also