Keysight 89600 VSA .NET API
AcquisitionStatus Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > UserInputData Class : AcquisitionStatus Property


Glossary Item Box

Gets or sets the acquisition status feedback from the data source application.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property AcquisitionStatus As UserInputAcquisitionStatus
C# 
public abstract UserInputAcquisitionStatus AcquisitionStatus {get; set;}
C++/CLI 
public:
abstract property UserInputAcquisitionStatus AcquisitionStatus {
   UserInputAcquisitionStatus get();
   void set (    UserInputAcquisitionStatus value);
}

Remarks

This sets properties for all channels, and gets the property value of the first channel. Use Channels to get or set properties of individual channels.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also