Keysight 89600 VSA .NET API
UserInputSetupChannel Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : UserInputSetupChannel Class


Glossary Item Box

This interface is for channelized (on a per input channel basis) properties and methods for defining properties of the data source application.

Syntax

Visual Basic (Declaration) 
Public MustInherit Class UserInputSetupChannel 
   Inherits RemotableObject
   Implements IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged 
C++/CLI 
public ref class UserInputSetupChannel abstract : public RemotableObject, IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged  

Remarks

This interface is contained by elements in a UserInputSetupChannelCollection.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also