Keysight 89600 VSA .NET API
ContextCollection Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace : ContextCollection Class


Glossary Item Box

This collection contains the set of Context objects currently loaded in the application.

Object Model

ContextCollection ClassContext ClassContext Class

Syntax

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also