Keysight 89600 VSA .NET API
MeasurementControlAffectedMeasurementsSelection Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace : MeasurementControlAffectedMeasurementsSelection Enumeration


Glossary Item Box

Indicates which measurement(s) should be affected.

Syntax

Visual Basic (Declaration) 
Public Enum MeasurementControlAffectedMeasurementsSelection 
   Inherits System.Enum
C# 
public enum MeasurementControlAffectedMeasurementsSelection : System.Enum 
C++/CLI 
public enum class MeasurementControlAffectedMeasurementsSelection : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AllMeasurementsAll measurements should be affected.—
DataSourceMeasurementsOnly the measurement(s) associated with the DataSources should be affected.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also