Keysight 89600 VSA .NET API
StatusMessage Class Members
See Also  Properties 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace : StatusMessage Class

Glossary Item Box

The following tables list the members exposed by StatusMessage.

Public Constructors

 NameDescriptionMinimum SW Version
Public ConstructorStatusMessage ConstructorInitializes a new instance of the StatusMessage class.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyMessageGets details about the result.  —
Public PropertySourceNameGets the name of the source of the result.  —
Public PropertyStatusGets a value indicating the severity of the result.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also