Keysight 89600 VSA .NET API
Format Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > AllocationBase Class : Format Property


Glossary Item Box

Gets or sets the PUCCH format for the allocation/channel.

Syntax

Visual Basic (Declaration) 
Public Property Format As PucchFormatType
C# 
public PucchFormatType Format {get; set;}
C++/CLI 
public:
property PucchFormatType Format {
   PucchFormatType get();
   void set (    PucchFormatType value);
}

Property Value

The default value is PucchFormatType.Format1.

Remarks

This property is valid for PUCCH allocations only.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also