Keysight 89600 VSA .NET API
Agilent.SA.Vsa.Lte Namespace
See Also  Inheritance Hierarchy
Agilent.SA.Vsa.Lte.Interfaces Assembly : Agilent.SA.Vsa.Lte Namespace

Glossary Item Box

The Agilent.SA.Vsa.Lte namespace contains classes and enums to control  LTE demodulation analysis features.

Classes

 ClassDescription
ClassAllocation The Lte.Allocation class contains properties and methods to control each LTE allocation
ClassAllocationBase The Lte.AllocationBase class contains properties and methods that are common to LTE allocations and Channels. The Lte.AllocationBase class contains properties and methods that are common to LTE allocations and Channels.
ClassAllocationCollection The Lte.AllocationCollection class contains properties and methods to manipulate a collection of LTE Allocation objects.
ClassChannel The Lte.Channel class contains properties and methods that are common to UL channels and DL users. The Lte.Channel class contains properties and methods that are common to UL channels and DL users.
ClassDownlinkRateMatchPattern Strongly-typed downlink rate match pattern. All members are on the shared base class RateMatchPattern.
ClassDownlinkRateMatchPatternCollection Represents the configured downlink rate match patterns.
ClassDownlinkUser The Lte.DownlinkUser class contains properties and methods specific to LTE Downlink users.
ClassDownlinkUserCollection The Lte.DownlinkUserCollection class contains properties and methods to manipulate a collection of LTE DownlinkUser objects.
ClassLayer The Lte.Layer class contains properties and methods to control the behavior of each Layer of an LTE DownlinkUser.
ClassLayerCollection The Lte.LayerCollection class contains properties and methods to manipulate the collection of LTE Layer objects.
ClassMeasurementExtension The Lte.MeasurementExtension object contains properties and methods to control the LTE demodulation measurement features
ClassPrach The Prach class contains properties and methods to control the behavior of LTE PRACH channel.
ClassPucch The Pucch class contains properties and methods to control the behavior of LTE PUCCH channel.
ClassPusch The Pusch class contains properties and methods to control the behavior of LTE PUSCH channel.
ClassRateMatchPattern Defines an O-RAN Fronthaul WG4 rate match pattern that punctures specified resource elements during PDSCH (downlink) demodulation.
ClassSrs The Srs class contains properties and methods to control the behavior of LTE SRS channel.
ClassUplinkUser The Lte.UplinkUser class contains properties and methods specific to LTE Uplink users.
ClassUplinkUserCollection The Lte.UplinkUserCollection class contains properties and methods to manipulate a collection of LTE UplinkUser objects.
ClassUserCollection<T> The Lte.UserCollection class contains properties and methods that are common to the manipulation of a collection of downlink or uplink users.

Enumerations

 EnumerationDescription
EnumerationAnalysisBandwidthType Specifies the bandwidth and the number of resource blocks.
EnumerationAnalysisBoundaryType Specifies the analysis start boundary.
EnumerationAntennaArrayShape Specifies the Antenna Array Shape used for Beamforming Pattern/Gain measurement.
EnumerationAntennaPortType Specifies the antenna port number that the transmission takes place on (Downlink only).
EnumerationCellBeamSeparationMethod Enum type to specify the method to estimate beamforming weight.
EnumerationCellIdModeType Specifies the Physical-layer Cell Identity Mode (Downlink only).
EnumerationChannelConditionType Specifies the channel conditions to determine the UL spectrum flatness limits
EnumerationCyclicDelayDiversityType Specifies the Cyclic Delay Diversity (CDD) decoding to be applied to Spatial Multiplexed DL Shared Channels (PDSCH)
EnumerationCyclicPrefixLengthModeType Specifies the Cyclic-prefix length mode.
EnumerationDciDetectIncludeType Specifies the DCI Detection Include which allows user to specify which supported combination of DCI Format 1, 1B, 1D are present within measured signal
EnumerationDciFormat1Format1ADetectType Specifies which DCI Format a PDCCH with ambiguous length is to be decoded as.
EnumerationDownlinkMultipleAccessScheme Specifies the multiple access mode for Downlink
EnumerationDuplexModeType Specifies the duplex mode: FDD or TDD
EnumerationElementSpacingUnit Specifies the Antenna Element Spacing Unit used for Beamforming Pattern/Gain measurement.
EnumerationEMTCCoverageMode Specifies the coverage mode used for EMTC
EnumerationEqualizerTrainingModeType Specifies the Equalizer Training mode (Uplink only).
EnumerationEqualizerTrainingType Specifies the Equalizer Training method.
EnumerationEvmMinimizationType Specifies the EVM Minimization method to use.
EnumerationFofdmFilterSelection Specifies the filter type used for 5G F-OFDM
EnumerationFofdmFilterWindow Specifies the window type used for 5G F-OFDM window filtering
EnumerationFofdmFilterWindowLengthMode Specifies the window length mode used for 5G F-OFDM window filtering if it is manual mode, the filter transition bandwidth is grayed out and determined by the filter length if it is auto mode, the filter length is determined by the transition bandwidth
EnumerationFrameNumberType Specifies which frame the allocation is located in.
EnumerationFrequencyHoppingType Specifies the Freq Hopping Type for PUSCH.
EnumerationInputChannelType Specifies the measurement input channel.
EnumerationLinkDirectionType Specifies the link direction.
EnumerationMimoDecodingType Specifies what type of MIMO decoding to apply to DL channels.
EnumerationModulationFormatType Specifies the modulation format used by data channels.
EnumerationMUSTCategoryType Specifies the multiuser superposition transmission scheme
EnumerationMUSTSICModeType Specifies the signal interference cancellation mode used in multiuser superposition transmission scheme measurement
EnumerationNumberOfCodewordsType Specifies the Number of Code words to be decoded from Spatial Multiplexed DL Shared Channels (PDSCH)
EnumerationNumberOfCsiRsPortsType Specifies the number of CSI-RS ports
EnumerationNumberOfLayersType Specifies the Number of Layers to be decoded from Spatial Multiplexed DL Shared Channels (PDSCH)
EnumerationNumberOfPositioningRsSubframesType Specifies the number of consecutive DL sub-frames in which Positioning RS is transmitted.
EnumerationNumberOfTXAntennasType Specifies the total number of tx antenna ports for currently configured transmission system (Downlink only).
EnumerationOrthogonalCoverCodeType Specifies the Orthogonal Cover Code used by the PUSCH DMRS sequence
EnumerationOSIndexType Specifies the index for the Orthogonal Sequence in the PUCCH user channel allocation.
EnumerationPbchBitVectorSelectType Specifies the PBCH Bit Vector Selection that determines the PBCH bit values displayed in Decoded Symbol Table trace
EnumerationPcfichBitVectorSelectType Specifies the PCFICH Bit Vector Selection that determines the PCFICH bit values displayed in Decoded Symbol Table trace
EnumerationPdcchBitVectorSelectType Specifies the PDCCH Bit Vector Selection that determines the PDCCH bit values displayed in Decoded Symbol Table trace
EnumerationPdschBitVectorSelectType Specifies the PDSCH Bit Vector Selection that determines the PDSCH bit values displayed in Decoded Symbol Table trace
EnumerationPdschCellSpecificRatioType Specifies the PDSCH Cell Specific Ratio p_B/p_A
EnumerationPdschIQReferenceGenerationModeType Specifies the IQ reference constellation generation mode for PDSCH
EnumerationPhichAllocationType Specifies the PHICH Allocation size to be used for PHICH resource element group mappings.
EnumerationPhichDurationType Specifies the PHICH Duration mapping method to be used for sub-frames containing 3 PDCCH symbol allocation.
EnumerationPhichMIDefinitionType Specifies the definition of m(i) to define the specific PHICH configuration for different sub-frames.
EnumerationPilotPrsType Specifies the pseudo-random sequence used for Reference Signal generation (Downlink only).
EnumerationPositioningRsPrecodingType Specifies if the signals Positioning RS (PRS) resource elements have precoding applied.
EnumerationPrachCyclicShiftSetType Specifies the PRACH cyclic shift set
EnumerationPucchBitVectorSelectType Specifies the PUCCH Bit Vector Selection which determines PUCCH bit values are displayed in Decoded Symbol Table trace
EnumerationPucchFormatType Specifies the PUCCH format type
EnumerationPuschBitVectorSelectType Specifies the PUSCH Bit Vector Selection which determines PUSCH bit values are displayed in Decoded Symbol Table trace
EnumerationPuxchTddAckNackFeedbackModeType Specifies the PUSCH/PUCCH TDD Ack/Nack Feedback Mode used by VSA to decode PUSCH and PUCCH HARQ Ack/Nack bits.
EnumerationRateMatchPatternSlotPatternPeriodicity Enum value indicating the length of the slot-pattern repetition window over which the slot-pattern bitmap applies.
EnumerationRBAutoDetectModeType Specifies the RB Auto Detect Mode which determines the method used to determine valid PDSCH RB allocations to be measured
EnumerationSharedChannelDecoderType Specifies what type of decoding should be applied to DL Shared Channels like PDSCH.
EnumerationSpecialSubframeConfigurationType Specifies the Dw/GP/Up Length for TDD.
EnumerationStandardsType Specifies the Preset-To-Standard Bandwidth.
EnumerationSymbolTimeAdjustmentMode Specifies the Symbol Time Adjust method used for EVM measurements.
EnumerationSynchronizationSignalAntennaPortType Specifies the P-SS/S-SS Antenna Port or Ports used for synchronization signal transmission
EnumerationSynchronizationSignalPrecodingType Specifies if the sync signals have precoding applied.
EnumerationSynchronizationTypeSelection Specifies which channel/signal to use for synchronization
EnumerationTransmissionModeTypes Specifies which Transmission Modes are included, so that decoding of the appropriate DCI Format may be attempted.
EnumerationUersScramblingId Specifies the scrambling ID used for UE-specific RS
EnumerationUersWeightsDisplayModeType Specifies the format of UE-specific RS weights display
EnumerationUplinkDownlinkAllocationType Specifies the Uplink/Downlink configuration type for TDD.
EnumerationUplinkMultipleAccessScheme Specifies the multiple access mode for Uplink
EnumerationWindowLengthModeType Specifies the EVM Window Length method used for EVM measurements.

See Also