| Visual Basic (Declaration) | |
|---|---|
Public Property SlotEnd As Integer | |
| C# | |
|---|---|
public int SlotEnd {get; set;} | |
Property Value
The default value is 0. The minimum value is 0 and the maximum is 19.SlotEnd has to be greater than or equal to SlotStart
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)