Keysight 89600 VSA .NET API
AllocationCollection Class
Members  See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : AllocationCollection Class


Glossary Item Box

The Lte.AllocationCollection class contains properties and methods to manipulate a collection of LTE Allocation objects.

Object Model

AllocationCollection ClassAllocation ClassAllocation Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class AllocationCollection 
   Inherits Agilent.SA.Vsa.RemotableCollection(Of Allocation)
   Implements Agilent.SA.Vsa.ICollectionBase, Agilent.SA.Vsa.ICollectionBase(Of Allocation), Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyCollectionChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3 

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also