Keysight 89600 VSA .NET API
AntennaArrayShape Enumeration
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : AntennaArrayShape Enumeration


Glossary Item Box

Specifies the Antenna Array Shape used for Beamforming Pattern/Gain measurement.

Syntax

Visual Basic (Declaration) 
Public Enum AntennaArrayShape 
   Inherits System.Enum
C# 
public enum AntennaArrayShape : System.Enum 
C++/CLI 
public enum class AntennaArrayShape : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
LinearLinear antenna array.—
RectangularRectangular plane array.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Remarks

Allows user to select what kind of shape the antenna array is.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 22.20

See Also