Keysight 89600 VSA .NET API
AntennaPortType Enumeration
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : AntennaPortType Enumeration


Glossary Item Box

Specifies the antenna port number that the transmission takes place on (Downlink only).

Syntax

Visual Basic (Declaration) 
Public Enum AntennaPortType 
   Inherits System.Enum
C# 
public enum AntennaPortType : System.Enum 
C++/CLI 
public enum class AntennaPortType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Port0Transmission is on Antenna port number 0.—
Port1Transmission is on Antenna port number 1.—
Port2Transmission is on Antenna port number 2.—
Port3Transmission is on Antenna port number 3.—
Port4Transmission is on Antenna port number 4.—
Port5Transmission is on Antenna port number 5.—
Port6Transmission is on Antenna port number 6.—
Port7Transmission is on Antenna port number 7.—
Port8Transmission is on Antenna port number 8.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also