Keysight 89600 VSA .NET API
Channel Class
Members  See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : Channel Class


Glossary Item Box

The Lte.Channel class contains properties and methods that are common to UL channels and DL users. The Lte.Channel class contains properties and methods that are common to UL channels and DL users.

Object Model

Channel ClassAllocationCollection ClassAllocation ClassAllocation Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class Channel 
   Inherits AllocationBase
   Implements Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3 
C# 
public abstract class Channel : AllocationBase, Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3  
C++/CLI 
public ref class Channel abstract : public AllocationBase, Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also